Task_Control

Task_Control

Address: 22950 (59A6)
Type: WORD
Access: Write Only
Unit: --
Range:

0 to 263

Byte 1 Value Byte 0

Task Command

Task Number

 

Task Command

Byte 1 Value Description

0

Kill Task

1

Restart Task

 

Task Number

Byte 0 Value Description

0 - 7

Task Number

Default Value: --
Store Supported: No
Description: This object can be used to kill or restart a task.
Notes:

If whole tasks are killed the error 'End of Program Execution' is raised (F+6 on display).